Hi friends,
I am using using TMS320F28335 controller DMA channels.McBSP channels are interfaced with the DMA channels.Here McBSP channels A is configured as receiver and mapped to the DMA channel A.In this case we have fixed the DMA data transfer size as 5 words and McBSP will generate interrupt for every word transmission.In this case as the McBSP is interfaced with the DMA do we need to enable McBSP receiver interrupt (McbspaRegs.MFFINT.bit.RINT = 1;) or we have disable.Is DMA will take care of this interrupt inernally if we disable McBSP receiver interrupt.
Please suggest me which way we can interface DMA - McBSP to get proper data transfer.
Thanks & Regards
Vedant