Part Number: TMS320F28379D
Other Parts Discussed in Thread: C2000WARE, LAUNCHXL-F28379D



Tool/software:
Hello,
I am running the code for step-up flyback converter whose input is around 40V and output is 320V and operated from
Code Composer Studio
Version: 11.1.0.00011
When I run my converter, the target is disconnected from CCS, and I get the following message.
C28xx_CPU1: Trouble reading memory block at 0xa9fe on page 1 of length 0x2:(Error -150 @0x0) One of the FTDI driver functions used during configuration returned a invalid status
C28xx_CPU1: Trouble Halthing Target CPU:( Error -150 @0x0) One of the FTDI driver functons used during configration returned a invalid status or an error
C28xx_CPU1: JTAG communication Error:( Error -150 @0x0) One of the FTDI driver functons used during configration returned a invalid status or an error
C28xx_CPU1: Failed to remove the debug state from the target before disconnecting. There may still be breakpoint op-codes embedded in program memory
Thanks and regards