Other Parts Discussed in Thread: TMS320F28035
Hello,
I have two questions. could you tell me about ?
Question 1: Now, using TMS320F28035 for control digital power and servo motor. I want to avoid short ciruit of high-side and low-side MOSFET in Power on sequencing. i've already used oscilloscope for measure waveform at Power on. There are a case high-side and low-side MOSFET is ON simultaneously cause short-circuit.
In SPRS584D 6.9. Power Sequencing timing chart (Page 103) as following:

Fig 1. Power Sequencing
GPIOs-state from power on to finish reset stage, All GPIOs as input, but state its is denpend on internal PU/PD. so , before reset, How GPIOs is pull-up/pull-down?
Question 2: in SPRUGL8B (page 97), GPIO0-GPIO11 is disable and GPIO12-GPIO44 is enable the internal pullup (After reset). as fig1, can use internal pullup for GPIO34, GPIO37 so that select Boot Mode?