Part Number: TMS320F28035
Tool/software:
Hi,
I am using TMS320f28035 for driving motor control with PMSM sensored. How can i limit the current of main bara? Is there any method for this using Id, Iq values or anything
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS320F28035
Tool/software:
Hi,
I am using TMS320f28035 for driving motor control with PMSM sensored. How can i limit the current of main bara? Is there any method for this using Id, Iq values or anything
Hi Yavuz,
Could you check this Q&A on MathWorks forum and see if it is helpful? Thanks!
https://www.mathworks.com/matlabcentral/answers/2129026-dc-current-limitation-in-foc-of-pmsm
Thanks,
Jiaxin
/*--------------------------DC Current Limit Code Snippet depend on SpeedRPM--------------------------*/
if (DC_Bara_Current_value_mA > DC_BARA_Current_max_limit)
{
if (limitHizAtamaSwitch == 0)
limitedSpeedRPM = YENI_REF_HIZ_FROM_RS422; // speed command assign to limitedRPM value when dc calculated value surpass the limit current value
limitHizAtamaSwitch = 1; //for once assign
akimHizLimitleyici = 1; // for doesnt assign new command speed value in control algorithm
limitedSpeedRPM -= 0.1; // decreasing 0.1RPM every loop
SpeedRef = _IQ(limitedSpeedRPM / speed1.BaseRpm); // for new proccessing value for speed
}
else if (DC_BARA_Current_max_limit - DC_Bara_Current_value_mA < 150.0) //schmitt zone for 150ma
{
if (limitedSpeedRPM > YENI_REF_HIZ_FROM_RS422)
akimHizLimitleyici = 0; // In hysteresis zone if new RPM value is low from limited RPM valu, it run
else
akimHizLimitleyici = 1; // In hysteresis zone if new RPM value is high from limited RPM valu, it doesnt run
}
else // normal proccesing
{
limitHizAtamaSwitch = 0; //for new RPM value assign
akimHizLimitleyici = 0;
}
/*-----------------------------------------------------------------------------------------------------------*/
Here my code for current limit depends on speed RPM.
I try to limit DC bara current with speed control of command value but my oppinion there can be another way with control id iq max min parameters. I already calculate DC bara with shunt resistor. If I find out how Id Iq values gives us how much current(their values come with per unit ), I can control them. And also they change through wiht DC bara voltage I know.