Part Number: TMS320F28388D
Tool/software:
I replicated fsi_ex1_loopback_cpucontrol, using external loopback. Since I am using the temporary hw I can work at a frequency of 1 Mhz maximum, using tx and rx in fiber optics
I have 3 questions:
-What can trigger the end of frame flag error event, see figure?
-Why doesn't the interrupt related to the receive go off?
-I have sometimes appeared the buffer underrun problem, do you know how to solve it and what it refers to?
The code is the same as the one made available in the SDK.
I can provide more info if needed.
Thanks in advance