This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDSCNCD28388D: Error #10234-D: unresolved symbols for vectortableflash on blinky demo for cm flash

Part Number: TMDSCNCD28388D
Other Parts Discussed in Thread: C2000WARE,

Tool/software:

Hi,

I have this error when building the cm flash for blink the led with the demo, I have controlled the code, the compiler and other task and are correct it's strange that doesn't see the vector table flash that i'ts defined on startup_cm.c

13] undefined        first referenced
[14]  symbol              in file     
[15] ---------        ----------------
[16] vectorTableFlash ./device/cm.obj
 
[17]error #10234-D: unresolved symbols remain
[18]error #10010: errors encountered during linking; "led_ex1_c28x_cm_blinky_cm.out" not built
 
[19]>> Compilation failure
[20]makefile:145: recipe for target 'led_ex1_c28x_cm_blinky_cm.out' failed
[21]gmake[1]: *** [led_ex1_c28x_cm_blinky_cm.out] Error 1
[22]makefile:138: recipe for target 'all' failed
[23]gmake: *** [all] Error 2
[24]**** Build Finished