Part Number: TMS320F28377D
Other Parts Discussed in Thread: C2000WARE
Tool/software:
The two 28377D devices communicate via serial ports.
The communication parameters are configured as follows: The baud rate is set to 115200, the RX FIFO is configured to 8 bits, and the communication is performed using an interrupt-based method.
The transmitter sends 8 bytes each time.When the first frame of 8 data bytes is received, the operation is normal.Starting from the second transmission, data offset errors will occur during reception.
The serial port configuration is as follows::
void InitSciBFIFO()
{
// ScibRegs.SCICCR.all = 0x0007; // 1 stop bit, No loopback
// // No parity,8 char bits,
// // async mode, idle-line protocol
ScibRegs.SCICCR.all = 0x0087; // 1 stop bit, No loopback
// No parity,8 char bits,
// async mode, idle-line protocol
ScibRegs.SCICTL1.all = 0x0003; // enable TX, RX, internal SCICLK,
// Disable RX ERR, SLEEP, TXWAKE
ScibRegs.SCICTL2.all = 0x0003;
//ScibRegs.SCICTL2.bit.TXINTENA = 0;
ScibRegs.SCICTL2.bit.RXBKINTENA = 1; //Enable SCIB _RX
//
// SCIA at 9600 baud
// @LSPCLK = 50 MHz (200 MHz SYSCLK) HBAUD = 0x02 and LBAUD = 0x8B.
// @LSPCLK = 30 MHz (120 MHz SYSCLK) HBAUD = 0x01 and LBAUD = 0x86.
// @LSPCLK = 25 MHz (100 MHz SYSCLK) HBAUD = 0x01 and LBAUD = 0x45.
ScibRegs.SCIHBAUD.all = 0x0000; // @LSPCLK = 50 MHz 115200
ScibRegs.SCILBAUD.all = 0x0036;
// ScibRegs.SCIHBAUD.all = 0x0000; // @LSPCLK = 50 MHz 1M
// ScibRegs.SCILBAUD.all = 0x0006;
ScibRegs.SCIFFTX.bit.TXFIFORESET = 0;
ScibRegs.SCIFFRX.bit.RXFIFORESET = 0;
ScibRegs.SCICTL1.all = 0x0023; // Relinquish SCI from Reset
// Enable SCIFIFO
ScibRegs.SCIFFTX.all = 0xF040; //Disable FIFO Using 4 Enable FIFO Using 6
ScibRegs.SCIFFRX.all = 0x2068; //FIFO interupter level 8 interrupter level == 5
ScibRegs.SCIFFCT.all = 0x0;
ScibRegs.SCIFFTX.bit.TXFFINTCLR = 1; //Avoid PowerUp DataTX
ScibRegs.SCIFFTX.bit.TXFFIENA = 0; //Avoid PowerUp DataTX
}
The interrupt processing
__interrupt void ScibRxfifo_isr(void)
{
volatile static Uint32 ScibInteruptimes = 0;
ScibInteruptimes++;
if (SCIB_Recdata.uStatus != FINISH)
{
while(ScibRegs.SCIFFRX.bit.RXFFST)
{
SCIB_Recdata.uData[SCIB_Recdata.uIndex++] = ScibRegs.SCIRXBUF.all&0xff;
}
//update sci recevie status and set interrupt interval.
SCIB_Recdata.uStatus = WORKING;
SCIB_Recdata.ticker = SCIB_Recdata.spacetime;
}
ScibRegs.SCIFFRX.bit.RXFFOVRCLR = 1; // Clear Overflow flag
ScibRegs.SCIFFRX.bit.RXFFINTCLR = 1; // Clear Interrupt flag
ScibRegs.SCIFFRX.bit.RXFIFORESET = 1;
// Issue PIE ack
PieCtrlRegs.PIEACK.all = PIEACK_GROUP9; // Issue PIE ACK PIEACK_GROUP9
}
The specific example is as follows:
When I send 0x01 0x47 0x6A 0x00 0x00 0x00 0x00 0x55

The observation is made in the interrupt function of the receiver.

The recive data is 0x00 0x55 0x01 0x47 0x6A 0x00 0x00 0x00

The above configuration has been applied to the project of communication between the DSP and ARM, and there are no issues during the communication process. However, while debugging the communication between two DSPs, Do you have any suggestions for solving this issue?