This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F280039: Basic Configuration

Part Number: TMS320F280039

Tool/software:

Hi expert,

Here are several questions for F280039 basic configuration:

1. TMS320F280039 PZ (LQFP, 100), TMS320F28P650DK6 PTP (HLQFP, 176), is it correct that the basic configurations of these two MCUs are only reset, clock, power supply, and JTAG?

2. I didn't see the hardware configuration section about boot, is it not needed?

3. Is there anything else that needs to be configured?

Thanks

Joyce

  • Hi Joyce,

    I'm not sure what you mean by "basic configuration". Could you please elaborate on what your goals are for this setup? Are you just wanting to initialize the devices? Are any peripherals being used? The bootrom will run through its initialization, the rest is up to your boot pin setup and code. Is there a specific boot mode you are needing to use?

    Best Regards,

    Allison