This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDM-1000: Vienna Rectifier One or two phase power failure

Part Number: TIDM-1000

Tool/software:

Helle Everyone,

I am  working on designing a 3-phase Vienna rectifier with the Neutral Point Clamped (NPC) topology and considering using SVPWM for control. I am  having trouble predicting how the control algorithm will behave if one or two phases fail during normal operation. Specifically, I am  unsure how to write a control algorithm that ensures the circuit continues to function properly even if one phase is lost. Can you help with this? How would we write a control algorithm so that the circuit operates without significant impact when one of the phases goes down