Part Number: TMS320F280039C
Other Parts Discussed in Thread: SYSCONFIG
Tool/software:
Hello,
I have a question about the Flash API and configuring a linker cmd file in sysconfig. I’m currently working on migrating a project from running in RAM to running in Flash on a C2000 microcontroller. However I’m getting an illegal interrupt error when my code reaches some of the Flash API functions, which leads me to believe that my FlashAPI is being run from Flash instead of RAM. I see in the flash API example that the linker command file has this line:

However, I was wondering how this could be replicated using the linker command file section in SysConfig.
Thanks,
Justin