Part Number: TMDSHVMTRINSPIN
Tool/software:
Hi,
I found the shoot through protection circuit as shown below.

Is there any single IC available from TI to implement this logic
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMDSHVMTRINSPIN
Tool/software:
Hi,
I found the shoot through protection circuit as shown below.

Is there any single IC available from TI to implement this logic
I'm not aware of a chip with this functinality.
This is just a redundant design for protection. Generally, the C2000 MCU can generate the deadband so this protection is not needed in most cases. Only a few high-end applications use such protections, and typically an isolation driver would support this feature without any additional IC.
maybe you should switch a C2000 MCU
here is an example of a gate driver with this feature