Part Number: TMS320F28377D
Other Parts Discussed in Thread: C2000WARE
Tool/software:
Dear TI forum,
i am currently developing on on a F28377D using C2000Ware_5_03_00_00. In order to access the SD Card, i am using the fatfs and sdspi library provided in C2000Ware. As long as the SD Card is inserted, everything works totally fine. Whenever I remove the card and then try to access it again, or when I remove and put it back in, the file sdspi.c throws an ESTOP0 in line 417.
/* Single block read */
if (sectorCount == 1) {
sendCmdResult = sendCmd(handle->spiHandle, CMD17, sector);
recvStatus = recvDataBlock(handle->spiHandle, buf, SD_SECTOR_SIZE);
if ((sendCmdResult == 0) &&
recvStatus) {
status = SD_STATUS_SUCCESS;
}
else
{
ESTOP0;
}
}Why does the library behave this way and does not just return an SD_STATUS_ERROR, as done in many other parts of that file? Is there any way to prevent that behavior, since it halts the entire microcontroller?
Thank you very much for your response in advance!
Kind regards