Part Number: TMS320F28379D
Other Parts Discussed in Thread: CONTROLSUITE, C2000WARE
Tool/software:
Dear Experts and Gurus,
I have been working on a project and I could run CLA and its math library. Here are the strange observations I made with the CLA wrt controlsuite and C2000ware.
1. CLA gets triggered with the F2837xD_Headers_nonBIOS_cpu1.cmd that is available in the ControlSuite, but does not work with C2000ware file.
2. Even if I wanted to to move on with the controlsuite version which successfully triggers the CLA, there are some warning related to ADCresults that are flagged. Finally in the runtime, no adc value is returned to the result registers.
3. With C2000ware there are no such warning as shown in the image, but CLA doesn't get triggered.

Here is the project (ControlSuite's C2000ware F2837xD_Headers_nonBIOS_cpu1) that triggers the CLA. Please check with the C2000ware version on you computer.pwm_adc_cla.zip
Regards,
Rajesh.