This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28027: SCI module

Part Number: TMS320F28027

Tool/software:

Hi Sir  : 

The SCI module of the TMS320F28027 chip we are currently using has a low RX pin for some reason during transmission. Theoretically, this low level will trigger the SCIRXST.bit.BRKDT register in the 28027 chip to be set to 1,
But after testing, we found that only a very small number of chips produce this error flag bit. We would like to understand the mechanism of this flag bit generation (why is it low when I send it? Most boards do not produce this flag bit, so let's do some abnormal judgment processing).
Because according to the specifications (triggering when 10 BITs are detected) and the waveform we tested, it should be generated. Please help analyze and answer this question. Thank you.
Blue: Receive RX, yellow: Enable RE, red: Send TX
Note: (The high level stage of the yellow enable RE signal is the transmission stage). During the transmission stage, our RX becomes low level, which theoretically should generate the BRKDT flag. However, we have tested that only a very small number of boards produce this signal.

  • Hi Anson,

    What does your setup currently look like? What is the device that you are communicating with?

    There are some non-deterministic timings in the SCI module, so it is possible that you will need to wait longer than the 10 low Bits before break detect flag is made

    Regards,

    Peter