This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28375D: ADC Simultaneous sampling sample and hold

Part Number: TMS320F28375D

Tool/software:

Hi Experts,

After working on F28379D, I would like to use F28375D for my final design because of its 100pin version that makes PCB design simpler. Unlike 4 ADCs on F28379D, F28375D has got only 2 ADCs, as a consequence, does simultaneous sampling(3 phase voltages and currents for instance) could be compromised?

In F28379D, each phase voltage can be connected to each ADC, so simultaneous sampling can be achieved by triggering 3 ADCs simultaneously.

However, I see the Sample and Hold section in the ADC module and I wonder if the simultaneous sampling can be achieved using a single ADC.

Thanks and Regards,

Rajesh.