Other Parts Discussed in Thread: C2000WARE
Tool/software:
Hello all,
I used the LAUNCHXL-F28069M kit with CCS version 12. But now that version 20 has been released, I wanted to try it out. I usually create a blank project with an empty .c file and in version 12 that would automatically add the 28069_RAM_lnk.cmd file. I would then add the necessary files and edit the project settings to add the header files.
With CCS version 20.1, it automatically downloads C2000Ware version 5.04 to import the project. But then when I choose "2806x Example in C" I get this error:

The same error also appears with "2806x Example in CPP".
Any idea what needs to be done?