This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F280039C: Pin width of PN package

Part Number: TMS320F280039C

Tool/software:

Hi champs,

I am asking this for our customer.

In P269 of the datasheet, it shows 80-QFP PN package.

The user is concerned about the pin width and wants to confirm because they need to tune for surface mount.

1. The pin width below means that it can range from 0.17 to 0.27 mm.

Is our understanding correct?

2. That is, the average pin width is 0.22 mm and the difference can be +- 0.05 mm (up to 22%).

Is our understanding correct?