Part Number: TMS320F28P550SG
Other Parts Discussed in Thread: SYSCONFIG
Tool/software:
Does the F28P55x SCI support a communication rate of at least 8 Mbps? The maximum communication rate is calculated as 150 MHz / 16 = 9.375 Mbps, but does this mean it is achievable for the F28P55x? Additionally, I would like to know which other low-cost MCU models in the C2000 series support an SCI rate of at least 8 Mbps. I am considering the F29003x/F280015x, which has a clock frequency of 120 MHz. Is it possible for this model to achieve an SCI rate of no less than 8 Mbps?