Part Number: TMS320F280049C
Tool/software:
Dear Experts,
As we know, the erase/write/fetch speeds for Flash depend on FCLK, which is configured by the RWAIT register. However, I would like to confirm whether the speeds for erase, write, and fetch are calculated as SYSCLK / (RWAIT + 1).
For example, if SYSCLK is 100 MHz and RWAIT is set to 4, can I confirm that both erase and write speeds are 20 MHz?
If not, what are the actual speeds?
Thanks and regards,
CC Liu