Part Number: TMS320F2800156-Q1
Tool/software:
Hello guys,
This is my first TI forum for help.
I'm doing LIN Slave mode communication with TMS320F2800156
When I did the signal injection test for the LIN conformance test, I met some problems.
Not only the bit error of the inter-byte cannot be detected, but also the bit error of the normal data byte cannot be detected.
1.All bit error of inter-byte detection are failed.
2.Pars of bit error of data byte(Byte7~8) detection are failed.
In particular, it should be noted that although the bit error of Byte1~6 is passed, this is because I added the comparison of Rx data and Tx Data in the software.
If I just judge the Bit error flag, bit error of Byte1~6 also faied,except stop bit error.(I mean the bit error flag can recognize the stop bit error, which is why all stop bit errors can be detected).
The picture below shows my MCU setup and test results.
Looking forward to your help,thanks!