This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F280025C: Getting started with ACIM FOC development

Part Number: TMS320F280025C
Other Parts Discussed in Thread: TIDM-02017, C2000WARE

Tool/software:

Dear C2000 Team,

My AC induction motor has te following specs:

  • 4200 watt
  • 3200 RPM
  • 3x32 Vrms
  • 102 A (nominal)
  • CF: 110Hz
  • Cosfi: 0.85

The motor contains two temperature sensors and one 64ppr encoder.

I would like to start development for this motor with FOC control. I think it is best to start with some example code running on a development kit.

Can you recommend the correct hardware to get started?