Part Number: TMS320F280025
Tool/software:
Hi,
I'm using the MotorControl SDK V5.0.2 with the universal motor control example with a ACIM motor. Now it seems to work fine, expect there is a problem with FWC.
FWC seems only to work in the positive speed direction and it increases the magnetic current in the opposite direciton. Is this a bug? When I do the following, it works,
but I'm not sure if MTPA then still work:
in motor1_drive.c (use fabsf of IsRef instead of directly IsRef seems to solve the issue):

Thanks