This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28379D: Is EMIF1 supported in PTP (176) package.

Part Number: TMS320F28379D

Tool/software:

I am using TMS320F28379D, EMIF1 is being used for controlling a parallel 16 bit NOR Flash. I am using a PTP (176) package for which the default configuration as well as custom configurations throw error as some of the address pins of the EMIF conflict with its own DQM pins. Is EMIF1 supported by the PTP package or do we need to use ZWT 336 pin package.