Other Parts Discussed in Thread: AM263P4
Tool/software:
Hello,
We would like to develop a motor controller using the F29H859 C2000 F29 processor that can drive two AC motors for traction and one motor for pump applications which can be either AC or DC (BLDC, PMSM, ACIM).
Do you have software libraries available for these applications, and is the processor's performance sufficient for this use case?
Additionally, we want our system to achieve PLd as per ISO 13849.
We will be using the TPS653860 PMIC.
Can we achieve PLd as per ISO 13849 directly with the TPS653860 and F29H859, or do we need an additional MCU as test equipment?
Best regards,
Egemen