Part Number: TMS320F28388D
Tool/software:
Hello,
I was following a resource to test EtherCAT and specifically following the CPU1 Echoback Solution Example. I'm using TwinCAT as the resource suggests. Well I got to a point where I can see process data mapping on TwinCAT but everytime it comes up after a scan it shows an error with the device going from SAFEOP to OP

For reference I'm using SSC 5.12 since the document said this is the only version supported. Also I am using a controlCard for the F28388D.

I started debugging to see if I could find out why the device is unable to enter OP mode but I decided to reach out to you before I went in too far
Another issue: During the time I was debugging, I was clicking around TwinCAT in the state machine and I'm not sure if this is what caused my issue but suddenly I could no longer detect an EtherCAT device from either TwinCAT or SOEM. Eventually I just moved my ethernet cable over to the other slot and things appear to be working again, so I suppose it's either some hardware issue or the device is in a weird state that I cannot seem to fix. Wanted to get your thoughts on this to see if people have had this issue before.
Thanks,
Antonio