Tool/software:
Hi Ti team,
I'm using TIDM-1000 reference for my project which is having generator source as power supply
I kept switching frequency 200KHz. Control ISR running at 100Khz.
Case1: When I apply input voltage 200Vl-l with input frequency 128Hz, I'm able to boost 400VDC, When I increase DC bus voltage to >400 I'm not able to boost.
Case2: When I apply input voltage 300Vl-l with input frequency 180Hz, I'm not able to boost to any voltage I tried this voltage: 500VDC, 550, 600, 650.to
Are there any parameters to configure in this case.