Hi TI Community,
We are working with TMS320C2000 Development Tools, and the related control card is TMDSCNCD28335PGF R1.0.
In this kit there are two stations, each of which presents:
- 1 F28335 control card
- 1 docking station
- 1 AFE board
- 1 AC/DC 15V Power Supplier
We want to implement a PRIME MAC layer test, but we don't have understood if one of the two stations can implements Base Node functionality.
If we want to create a Base Node for our network, can we use only a single station? If not, which external device, not included in our kit, can be used?
Thanks, regards.