This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDM-02002: Alternative Push-Pull Transformer

Part Number: TIDM-02002

Tool/software:

Hello E2E Experts,

Good day.

I want to develop CLLLC resonant converter on the TI design file. But, I am facing problems to buy push-pull transformer whose part number is mentioned as 750317722. The lead time is much longer. I need it emergency supply for my project. Could you let me know alternative of this transformer for gate driver circuits that are compatible to the TI design files. I am providing the details of the transformer for gate driver circuit as follows

Part number: 750317722
Description: push-pull transformer, 320 uH, SMD
Turn ratio: 1: 3.9
Input voltage: 5 V
Output voltage: 19 V
Frequency: 500 kHz
Package Reference: 7.14 x 6.73 mm

Regards,

TICSC