Part Number: LAUNCHXL-F28379D
Tool/software:
Hello, I started off with the adc_ex_temp_sensor example that includes and adc in it that takes in measurements from ADCINA0 and I was attempting to modify it to also take in measurements from another pin. As I went about my attempt I noticed that the "while" loop that normally cycles until the buffer is full of adc readings, stops working (never exits the loop) when I attempt to add the other adc pin (ADC_SOC_NUMBER1). Why is this? Am I missing something in how I am initializing all this? Thanks.