Part Number: LAUNCHXL-F28P65X
Other Parts Discussed in Thread: C2000WARE
Tool/software:
Hello,
I have a question while using the C2000Ware_5_04_00_00 SDK.
( Example location: C:\ti\c2000\C2000Ware_5_04_00_00\libraries\communications\Ethercat\f28p65x\examples\f28p65x_cpu1_echoback_solution )
I am using the f28p65x_cpu1_echoback_solution example to test the basic operation of the EtherCAT Slave, and I am running only the provided example without any code modifications.
Currently, I have confirmed that it operates in the Operation state using TwinCAT as the EtherCAT Master.
While rebooting the board, I am monitoring the operation in the Operation state, but occasionally, the EtherCAT connection fails, and it remains in the Init state.
Has this issue occurred in the basic example, and were any modifications made to resolve it? Could you please advise on which areas I should check?
thanks.