This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28027F: TMS320F28027F

Part Number: TMS320F28027F
Other Parts Discussed in Thread: LAUNCHXL-F28027F, C2000WARE, , ENERGIA

Tool/software:

Can any one help me to work on i2c interface using bmp sensor of C2000 piccolo Launchxl-f28027f i have tried many way not getting please check 

  • Hi Kishor,

    As a starting point, you can refer to the I2C EEPROM example as a starting point for interfacing with a sensor. If you have any specific questions on the implementation, let me know and I can help.

    C:\ti\c2000\C2000Ware_5_04_00_00\device_support\f2802x\examples\structs\i2c_eeprom

    Best Regards,

    Aishwarya

  • Hi Aishwarya Rajesh

    "I've written the logic to interface the BMP280 sensor with the TMS320F28027F using I2C, but I'm not getting any output. Please take a look at the code and let me know what might be wrong."

    #include "DSP28x_Project.h"     // Device Headerfile and Examples Include File
    #include <stdio.h>              // For sprintf
    #include <stdint.h>             // For uint8_t, int16_t, etc.
    
    // BMP280 Definitions
    #define BMP280_ADDR 0x76        // BMP280 I2C address (0x76 if SDO is low, 0x77 if SDO is high)
    #define BMP280_CALIB_DATA_SIZE 24
    
    // BMP280 Calibration Data
    uint16_t dig_T1;
    int16_t dig_T2, dig_T3;
    uint16_t dig_P1;
    int16_t dig_P2, dig_P3, dig_P4, dig_P5, dig_P6, dig_P7, dig_P8, dig_P9;
    
    // Global variable for fine temperature calculation
    int32_t t_fine;
    
    // Function Prototypes
    void InitI2C(void);
    void BMP280_Init(void);
    void I2C_Write(uint8_t slave_addr, uint8_t reg_addr, uint8_t data);
    void I2C_Read(uint8_t slave_addr, uint8_t reg_addr, uint8_t *data, uint8_t length);
    void BMP280_ReadCalibrationData(void);
    void BMP280_ReadData(float *temperature, float *pressure);
    float compensate_T(int32_t adc_T);
    float compensate_P(int32_t adc_P);
    void InitSCI(void);
    void SCI_Print(char *str);
    
    // Main Function
    void main(void)
    {
        float temperature, pressure;
        char buffer[50];  // Buffer to store formatted strings
    
        // Initialize system
        InitSysCtrl();      // Initialize the system control
        InitI2C();          // Initialize I2C for BMP280 communication
        InitSCI();          // Initialize SCI for UART communication
    
        // Test UART communication
        SCI_Print("Hello, BMP280!\n");
    
        // Initialize BMP280 sensor
        BMP280_Init();
        BMP280_ReadCalibrationData();  // Read calibration data from BMP280
    
        while (1)
        {
            // Read temperature and pressure from BMP280
            BMP280_ReadData(&temperature, &pressure);
    
            // Format and send temperature data
            sprintf(buffer, "Temperature: %.2f °C\n", temperature);
            SCI_Print(buffer);
    
            // Format and send pressure data
            sprintf(buffer, "Pressure: %.2f Pa\n", pressure);
            SCI_Print(buffer);
    
            DELAY_US(1000000);  // Delay for 1 second
        }
    }
    
    // Initialize I2C module
    void InitI2C(void)
    {
        // Enable I2C peripheral clock
        SysCtrlRegs.PCLKCR0.bit.I2CAENCLK = 1;
    
        // Configure I2C pins (GPIO32 as SDA and GPIO33 as SCL)
        EALLOW;
        GpioCtrlRegs.GPBPUD.bit.GPIO32 = 0;    // Enable pull-up for SDA (GPIO32)
        GpioCtrlRegs.GPBPUD.bit.GPIO33 = 0;    // Enable pull-up for SCL (GPIO33)
        GpioCtrlRegs.GPBMUX1.bit.GPIO32 = 1;   // Configure GPIO32 as I2C SDA
        GpioCtrlRegs.GPBMUX1.bit.GPIO33 = 1;   // Configure GPIO33 as I2C SCL
        EDIS;
    
        // Initialize I2C
        I2caRegs.I2CMDR.all = 0x0000;          // Put I2C in reset state
        I2caRegs.I2CPSC.all = 6;               // Prescaler for 12.5 MHz SYSCLK
        I2caRegs.I2CCLKL = 10;                 // Low time = 10 * I2CPSC
        I2caRegs.I2CCLKH = 10;                 // High time = 10 * I2CPSC
        I2caRegs.I2CMDR.all = 0x0020;          // Master mode, 7-bit address, free data format
    }
    
    // Initialize BMP280 sensor
    void BMP280_Init(void)
    {
        // Set oversampling and mode
        I2C_Write(BMP280_ADDR, 0xF4, 0x27);  // Control measurement register: x1 temp, x1 pressure, normal mode
        I2C_Write(BMP280_ADDR, 0xF5, 0x00);  // Configuration register: filter off, standby time 0.5ms
    }
    
    // Write to BMP280 register
    void I2C_Write(uint8_t slave_addr, uint8_t reg_addr, uint8_t data)
    {
        I2caRegs.I2CSAR = slave_addr;          // Set slave address
        I2caRegs.I2CCNT = 2;                   // Set byte count (register address + data)
        I2caRegs.I2CDXR = reg_addr;            // Load register address
        I2caRegs.I2CDXR = data;                // Load data
        I2caRegs.I2CMDR.all = 0x6E20;          // Start condition, master transmitter mode
    
        uint16_t timeout = 10000;              // Timeout counter
        while (I2caRegs.I2CSTR.bit.ARDY == 0 && timeout--); // Wait for stop condition
        if (timeout == 0) {
            SCI_Print("I2C Write Timeout!\n");
        }
    }
    
    // Read from BMP280 register
    void I2C_Read(uint8_t slave_addr, uint8_t reg_addr, uint8_t *data, uint8_t length)
    {
        I2caRegs.I2CSAR = slave_addr;          // Set slave address
        I2caRegs.I2CCNT = 1;                   // Set byte count for register address
        I2caRegs.I2CDXR = reg_addr;            // Load register address
        I2caRegs.I2CMDR.all = 0x6E20;          // Start condition, master transmitter mode
    
        uint16_t timeout = 10000;              // Timeout counter
        while (I2caRegs.I2CSTR.bit.ARDY == 0 && timeout--); // Wait for stop condition
        if (timeout == 0) {
            SCI_Print("I2C Read Address Timeout!\n");
        }
    
        I2caRegs.I2CCNT = length;              // Set byte count for data
        I2caRegs.I2CMDR.all = 0x2C20;          // Start condition, master receiver mode
    
        unsigned char i;  // Declare loop variable
        for (i = 0; i < length; i++) {
            timeout = 10000;                    // Reset timeout for each byte
            while (I2caRegs.I2CSTR.bit.RRDY == 0 && timeout--); // Wait for receive ready
            if (timeout == 0) {
                SCI_Print("I2C Read Data Timeout!\n");
                break;
            }
            data[i] = I2caRegs.I2CDRR;         // Read data
        }
    }
    
    // Read BMP280 calibration data
    void BMP280_ReadCalibrationData(void)
    {
        uint8_t calib_data[BMP280_CALIB_DATA_SIZE];
        I2C_Read(BMP280_ADDR, 0x88, calib_data, BMP280_CALIB_DATA_SIZE);
    
        dig_T1 = (calib_data[1] << 8) | calib_data[0];
        dig_T2 = (calib_data[3] << 8) | calib_data[2];
        dig_T3 = (calib_data[5] << 8) | calib_data[4];
        dig_P1 = (calib_data[7] << 8) | calib_data[6];
        dig_P2 = (calib_data[9] << 8) | calib_data[8];
        dig_P3 = (calib_data[11] << 8) | calib_data[10];
        dig_P4 = (calib_data[13] << 8) | calib_data[12];
        dig_P5 = (calib_data[15] << 8) | calib_data[14];
        dig_P6 = (calib_data[17] << 8) | calib_data[16];
        dig_P7 = (calib_data[19] << 8) | calib_data[18];
        dig_P8 = (calib_data[21] << 8) | calib_data[20];
        dig_P9 = (calib_data[23] << 8) | calib_data[22];
    }
    
    // Read temperature and pressure data from BMP280
    void BMP280_ReadData(float *temperature, float *pressure)
    {
        uint8_t data[6];
        I2C_Read(BMP280_ADDR, 0xF7, data, 6); // Read pressure and temperature data
    
        int32_t adc_P = (data[0] << 12) | (data[1] << 4) | (data[2] >> 4);
        int32_t adc_T = (data[3] << 12) | (data[4] << 4) | (data[5] >> 4);
    
        *temperature = compensate_T(adc_T);
        *pressure = compensate_P(adc_P);
    }
    
    // Temperature compensation formula
    float compensate_T(int32_t adc_T)
    {
        int32_t var1, var2;
        var1 = ((((adc_T >> 3) - ((int32_t)dig_T1 << 1))) * ((int32_t)dig_T2)) >> 11;
        var2 = (((((adc_T >> 4) - ((int32_t)dig_T1)) * ((adc_T >> 4) - ((int32_t)dig_T1))) >> 12) * ((int32_t)dig_T3)) >> 14;
        t_fine = var1 + var2;  // Update t_fine for pressure compensation
        return (t_fine * 5 + 128) >> 8;  // Return temperature in °C
    }
    
    // Pressure compensation formula
    float compensate_P(int32_t adc_P)
    {
        int64_t var1, var2, p;
        var1 = ((int64_t)t_fine) - 128000;
        var2 = var1 * var1 * (int64_t)dig_P6;
        var2 = var2 + ((var1 * (int64_t)dig_P5) << 17);
        var2 = var2 + ((int64_t)dig_P4 << 35);
        var1 = ((var1 * var1 * (int64_t)dig_P3) >> 8) + ((var1 * (int64_t)dig_P2) << 12);
        var1 = (((int64_t)1 << 47) + var1) * ((int64_t)dig_P1) >> 33;
        if (var1 == 0) return 0;  // Avoid division by zero
        p = 1048576 - adc_P;
        p = (((p << 31) - var2) * 3125) / var1;
        var1 = ((int64_t)dig_P9 * (p >> 13) * (p >> 13)) >> 25;
        var2 = ((int64_t)dig_P8 * p) >> 19;
        p = ((p + var1 + var2) >> 8) + ((int64_t)dig_P7 << 4);
        return (float)p / 256.0;  // Return pressure in Pa
    }
    
    // Initialize SCI for UART communication
    void InitSCI(void)
    {
        // Enable SCI peripheral clock
        SysCtrlRegs.PCLKCR0.bit.SCIAENCLK = 1;
    
        // Configure SCI pins
        EALLOW;
        GpioCtrlRegs.GPAPUD.bit.GPIO28 = 0;    // Enable pull-up for SCITXDA (GPIO28)
        GpioCtrlRegs.GPAPUD.bit.GPIO29 = 0;    // Enable pull-up for SCIRXDA (GPIO29)
        GpioCtrlRegs.GPAMUX2.bit.GPIO28 = 1;   // Configure GPIO28 as SCITXDA
        GpioCtrlRegs.GPAMUX2.bit.GPIO29 = 1;   // Configure GPIO29 as SCIRXDA
        EDIS;
    
        // Initialize SCI
        SciaRegs.SCICCR.all = 0x0007;  // 1 stop bit, no parity, 8-bit data, idle-line protocol
        SciaRegs.SCICTL1.all = 0x0003; // Enable TX and RX, internal SCICLK
        SciaRegs.SCIHBAUD = 0x0001;    // Baud rate = 9600 (for 12.5 MHz SYSCLK)
        SciaRegs.SCILBAUD = 0x00E7;
        SciaRegs.SCICTL1.all = 0x0023; // Relinquish SCI from reset
    }
    
    // Print a string via SCI
    void SCI_Print(char *str)
    {
        while (*str) {
            while (SciaRegs.SCICTL2.bit.TXRDY == 0); // Wait for TX ready
            SciaRegs.SCITXBUF = *str++;               // Send character
        }
    }
    

  • Kishor,

    While I can't review code, let me know if you are seeing any output on the GPIOs or nothing at all? If there is no output on the pins, please take a look at the GPIO configurations and the physical connections between MCU and EEPROM. If there is output, then we can look at code configurations further. Please point me towards the specific portion of your code there may be an issue.

    Here is a thread that could be relevant: (+) TMS320F28027F: I2C sets Stop condition without being commanded to - C2000 microcontrollers forum - C2000Tm︎ microcontrollers - TI E2E support forums. There could be other E2Es as well on the forum that could be helpful.

    Best Regards,

    Aishwarya

  • Hi Aishwarya Rajesh,

     Referred the I2C EEPROM example instead of using external EEPROM i used BMP280 sensor and changed the slave address in the code. And also implemented the sci for debug prints. in that code just i implemented the i2c scanner code to found the i2c device connected by checking the loop from 0 to 128  devices. As bmp sensor, if i connected the SDO pin to ground it should get the 0x76 or if i connect to VCC it should get 0x77. it is not founding. why this actually all the initialization is done in the code.

    1.    Issues faced

    1)    Using sample BMP280 Sensor for any controller from Git.

    https://github.com/ebrezadev/BMP280-Barometric-Pressure-and-Temperature-Sensor-C-Driver/tree/main

    • From the above link download the zip file and add that four files in the program.
    • Right click on the project name and in pop window you will see the add files click on that and see the zip files where you download and extracted them, add source files to SRC and header file to INC.
    • Now need to implement the code in bmp280_low_level.c and main.c as per our MCU dependent.
    • In main function i2c initialization is done, sci implementation is done for debug print.
    • Flash the program.
    • It halt at the Read operation timeout print in read function, while debugging line by line it is Wait for data to be ready waiting for some time until timeout and prints the message Read operation timeout.
    • To overcome this first I need to check the whether i2c address is getting are not, then I implemented the i2c scanner code in main function called in while loop.
    • This scanner code is commented in main comment out the code to work on i2c scanner It while check the 128 device address.
    • BMP280 I2C device address is depend up on SDO pin if the SDO pin is connected to Ground it is 0x76 also if connected to VCC it is 0x77 also per connection it is connected to the ground.
    • The scanner function should detect the address of BMP280 sensor at 0x76.
    • But by checking this also device address is not getting.

    2)    Using logic analyzer check the I2C lines

    • To debug whether I2C lines are working or not-working.
    • Taken the I2C master code sample from git in which only contain the write function.

    https://github.com/kiranj26/C2000-Piccolo-F28027F-Projects/tree/main/examples/I2C/I2C_Master

    • Then connect the logic analyzer channels to SDA and SCL lines of Launchpad and ground to ground.
    • We found some raw data on SDA and SCL lines.
    • Then implemented the read function in this master code along with the debug prints and delay function calls it is also halted at the stop condition to complete the i2c communication completely but it is timeout without completing.

    3)    Worked on EEPROM Example

    • EEPROM Example program for external EEPROM device instead of that we are using the slave as BMP280 sensor and changed the slave address and implement the SCI message prints to debug what is getting.
    • Here also I didn’t get the output.
    • In this also program is halting in read function, read function is not working proper.

    4)    Energia IDE

    • Installed energia ide version 17.
    • Install code generator tool of version 6.2.6.
    • While installing give the path where eneria>>hardware>>tools>>c2000 and install.
    • Open ide and it is same as Arduino select board c2000-TMS320F28027F and serial port com11.
    • To check which com go to device drive>>port>>there we can see the com of our board if connect.
    • In this ide also implement the sample code of i2c scanner.

            The device is not found properly

    This is my bmp_low_level.c contains the read and write function.

    /*BMP280 barometric pressure and temperature sensor C Driver*/
    /*Reza Ebrahimi - https://github.com/ebrezadev */
    /*Version 1.0*/
    
    #include "bmp280.h"
    #include "sci.h"
    #include "i2c.h"
    //#include "DSP28x_Project.h"
    
    /* Writes an array (data[]) of arbitrary size (dataLength) to I2C address (deviceAddress),
       starting from an internal register address (startRegisterAddress) */
    void bmp280_write_array(uint8_t deviceAddress, uint8_t startRegisterAddress, uint8_t *data, uint8_t dataLength)
    {
        uint8_t i;
        EALLOW;
    
        // Enable I2C0 for writing
        I2caRegs.I2CMDR.bit.IRS = 1;  // Set to idle state
        I2caRegs.I2CSAR = deviceAddress;  // Set I2C device address
        I2caRegs.I2CCNT = dataLength + 1;  // Set number of bytes to send (register + dataLength)
    
        // Write start register address
        I2caRegs.I2CDXR = startRegisterAddress;
    
        for (i = 0; i < I2caRegs.I2CCNT; i++) {
            I2caRegs.I2CDXR = data[i];  // Write the data byte
        }
    
        // Start the I2C communication
        I2caRegs.I2CMDR.bit.IRS = 0;  // Initiate the transfer
        if (I2caRegs.I2CSTR.bit.BB == 1) {
    
        }
        if (I2caRegs.I2CSTR.bit.SCD == 1) {
    
        }
    
    
        EDIS;
    }
    
    void bmp280_read_array(uint8_t deviceAddress, uint8_t startRegisterAddress, uint8_t *data, uint8_t dataLength)
    {
        uint8_t i;
        uint32_t timeout = 200000;  // Set a higher timeout for read operation
    
        EALLOW;
    
        // Step 1: Write the register address (e.g., 0xD0 for chip ID)
        bmp280_write_array(deviceAddress, startRegisterAddress, NULL, 0);  // Write operation to select the register
    
        // Step 2: Perform a repeated start (restart the I2C bus to prepare for reading)
        I2caRegs.I2CMDR.bit.STT = 1;   // Initiate a restart condition (repeated start)
    
        // Wait for the I2C communication to complete
        timeout = 10000;  // Set timeout for wait after start condition
        while (I2caRegs.I2CSTR.bit.BB == 1 && timeout > 0) {  // Wait for the bus to be free (BB = bus busy)
            timeout--;
        }
    
        if (timeout == 0) {
            scia_msg("\r\nI2C bus busy, cannot start read operation.\0");
            EDIS;
            return;
        }
    
        // Step 3: Set up the I2C communication for reading data
        I2caRegs.I2CSAR = deviceAddress;  // Set I2C device address
        I2caRegs.I2CCNT = dataLength;     // Set number of bytes to read
        I2caRegs.I2CMDR.bit.IRS = 0;      // Start I2C communication for read operation
    
        // Step 4: Wait for the data to be ready and read the data byte by byte
        for (i = 0; i < dataLength; i++) {
            timeout = 200000;  // Adjust timeout limit as needed
    
            // Wait for data to be ready
            while (I2caRegs.I2CSTR.bit.RRDY != 1 && timeout > 0) {
                timeout--;
            }
    
            if (timeout == 0) {
                scia_msg("\r\nRead operation timeout.\0");
                EDIS;
                return;
            }
    
            // Read the data from the I2C data register
            data[i] = I2caRegs.I2CDRR;
        }
    
        // Step 5: End of I2C read operation
        scia_msg("\r\nRead operation successful.\0");
        EDIS;
    }
    
    
    
    
    /* A delay function for milliseconds delay */
    void delay_function(uint32_t delayMS)
    {
        uint32_t i;
        for (i = 0; i < delayMS; i++) {
            asm(" NOP");  // No operation (to create a small delay)
        }
    }
    
    /* Implements a power function (used in altitude calculation) */
    float power_function(float x, float y)
    {
        return power_function(x, y);
    }
    
      

    This is my main.c

    
    
    #include "DSP28x_Project.h"     // Device Headerfile and Examples Include File
    #include "clk.h"
    #include "gpio.h"
    #include "sci.h"
    #include "i2c.h"
    
    
    //// Function Prototypes
    void scia_echoback_init(void);
    void scia_fifo_init(void);
    void scia_xmit(int a);
    void scia_msg(char *msg);
    void scia_receive_string(char *buf, uint16_t max_len);
    
    
    // Globals
    CLK_Handle myClk;
    GPIO_Handle myGpio;
    SCI_Handle mySci;
    I2C_Handle i2cHandle;
    // Main
    
    
    
    void main(void)
    {
        InitSysCtrl();
        myClk = CLK_init((void *)CLK_BASE_ADDR, sizeof(CLK_Obj));
        myGpio = GPIO_init((void *)GPIO_BASE_ADDR, sizeof(GPIO_Obj));
        i2cHandle = I2C_init((void *)I2CA_BASE_ADDR, sizeof(I2C_Obj));
        mySci = SCI_init((void *)SCIA_BASE_ADDR, sizeof(SCI_Obj));
       //  Initialize GPIO
        InitI2CGpio();
            GPIO_setPullUp(myGpio, GPIO_Number_28, GPIO_PullUp_Enable);
            GPIO_setPullUp(myGpio, GPIO_Number_29, GPIO_PullUp_Disable);
            GPIO_setQualification(myGpio, GPIO_Number_28, GPIO_Qual_ASync);
            GPIO_setMode(myGpio, GPIO_Number_28, GPIO_28_Mode_SCIRXDA);
            GPIO_setMode(myGpio, GPIO_Number_29, GPIO_29_Mode_SCITXDA);
    
            scia_echoback_init();           // Initialize SCI for echoback
            scia_fifo_init();               // Initialize the SCI FIFO
            scia_msg("\r\nI2C PROGRAM START: \0");
    
             I2C_Init();
    
                while(1){
                    bmp280_init(); }
    
    }
    /* Initiates the I2C peripheral and sets its speed */
    
    void I2C_Init(void) {
        // Initialize I2C module
        I2caRegs.I2CMDR.all = 0; // Reset I2C
        I2caRegs.I2CPSC.all = 9; // Prescaler, set for 100kHz at 60MHz
        I2caRegs.I2CCLKL = 10;    // Set SCL low time
        I2caRegs.I2CCLKH = 5;    // Set SCL high time
        I2caRegs.I2CMDR.bit.FREE = 1; // Free run mode
        I2caRegs.I2CMDR.bit.MST = 1; // Set as master
        I2caRegs.I2CMDR.bit.IRS=1; // Enable I2C
        scia_msg("\r\nI2C_INITIALIZATION COMPLETED: \0");
    }
    
    
    //// I2C Scanner Function
    //void I2C_Scanner(void)
    //{
    //    uint32_t timeout = 10;  // Timeout counter
    //    uint8_t deviceAddress=100;
    //     for(deviceAddress;deviceAddress<128;deviceAddress++)
    //     {
    //        I2caRegs.I2CSAR = deviceAddress;// Set the slave address
    //
    //        // Send a start condition
    //       I2caRegs.I2CMDR.bit.STT = 1;  // Set start condition bit
    //
    //        // Wait for the start condition to complete
    //        while (I2caRegs.I2CSTR.bit.BB == 1 && timeout > 0)
    //           {
    //               timeout--;
    //           }
    //
    //           if (timeout == 0)
    //           {
    //               // Timeout occurred
    //               scia_msg("I2C start condition timeout.\r\n");
    //               return;
    //           }
    //
    //        // Check if the device responded
    //        if (I2caRegs.I2CSTR.bit.NACK == 0)
    //        {
    //            // Device found
    //            deviceAddress;
    //            scia_msg("\r\nDevice found: \0");
    //        }
    //
    //        // Send a stop condition
    //        I2caRegs.I2CMDR.bit.STP = 1;  // Set stop condition bit
    //
    //        // Wait for the stop condition to complete
    //        while (I2caRegs.I2CSTR.bit.BB == 1);  // Wait for bus to be free
    //}
    //}
    
    
    // Initialize SCI for echo-back communication
    void scia_echoback_init()
    {
        CLK_enableSciaClock(myClk);
    
        SCI_disableParity(mySci);
        SCI_setNumStopBits(mySci, SCI_NumStopBits_One);
        SCI_setCharLength(mySci, SCI_CharLength_8_Bits);
    
        SCI_enableTx(mySci);
        SCI_enableRx(mySci);
        SCI_enableTxInt(mySci);
        SCI_enableRxInt(mySci);
    
    #if (CPU_FRQ_60MHZ)
        SCI_setBaudRate(mySci, (SCI_BaudRate_e)194);
    #elif (CPU_FRQ_50MHZ)
        SCI_setBaudRate(mySci, (SCI_BaudRate_e)162);
    #elif (CPU_FRQ_40MHZ)
        SCI_setBaudRate(mySci, (SCI_BaudRate_e)129);
    #endif
    
        SCI_enable(mySci);
        return;
    }
    
     //scia_xmit - Transmit a character from the SCI
    void scia_xmit(int a)
    {
        while(SCI_getTxFifoStatus(mySci) != SCI_FifoStatus_Empty)
        {
        }
        SCI_putDataBlocking(mySci, a);
    }
    
    // scia_msg - Send a string via SCI
    void scia_msg(char *msg)
    {
        int i = 0;
        while(msg[i] != '\0')
        {
            scia_xmit(msg[i]);
            i++;
        }
    }
    
    // scia_fifo_init - Initialize the SCI FIFO
    void scia_fifo_init()
    {
        SCI_enableFifoEnh(mySci);
        SCI_resetTxFifo(mySci);
        SCI_clearTxFifoInt(mySci);
        SCI_resetChannels(mySci);
        SCI_setTxFifoIntLevel(mySci, SCI_FifoLevel_Empty);
    
        SCI_resetRxFifo(mySci);
        SCI_clearRxFifoInt(mySci);
        SCI_setRxFifoIntLevel(mySci, SCI_FifoLevel_4_Words);
        return;
    }
    
    // scia_receive_string - Receive a string over SCI
    void scia_receive_string(char *buf, uint16_t max_len)
    {
        uint16_t index = 0;
        uint16_t receivedChar;
    
        // Receive characters until we hit max_len or a newline/return character
        while(index < (max_len - 1))
        {
            while(SCI_getRxFifoStatus(mySci) < SCI_FifoStatus_1_Word)
            {
                // Wait for data to be available in the RX FIFO
            }
    
            receivedChar = SCI_getData(mySci);  // Get the received character
    
            if(receivedChar == '\r' || receivedChar == '\n')  // Newline/return ends the string
            {
                buf[index] = '\0';  // Null-terminate the string
                break;
            }
            else
            {
                buf[index] = receivedChar;  // Store the character
                index++;
            }
        }
    
        if (index == (max_len - 1))  // Ensure null-termination if max_len is reached
        {
            buf[index] = '\0';
        }
    }
    
    
    
    
    
    

  • Kishor,

    Could you confirm if you are seeing any output on the scope and share what you are seeing. I am not clear on that point. Also, make sure you have a pull up resistor connecting SDA and SCL to VDDIO at around 2.2 kOhms. Refer to this App Note for some more information as well: Interfacing EEPROM Using C2000 I2C Module

    Please also give me 1-2 days to look into this further and get back to you. 

    Best Regards,

    Aishwarya

  • HI Aishwarya Rajesh,

    I'm using 4.7kOhms  pull up resistor connecting SDA and SCL to VCC .

    output iam seeing

    read operation is timeout in bmp_low_level.c.

  • Kishor,

    Can you send an image of the reading on the oscilloscope.

    Best Regards,

    Aishwarya

  • Hi Aishwarya Rajesh,

    i have checked in logic Analyzer 

  • Kishor,

    Let me look into this further and get back to you.

    Best Regards,

    Aishwarya

  • Hi Aishwarya Rajesh,

    Thanks for this response i have detected bmp280 sensor chip id (i2c detected ) by this thread and now working on get bmp sensor data if any issues i will get back to you.

  • Kishor,

    Glad to hear, let me know if you have any other questions, and/or please mark this thread as resolved accordingly.

    Best Regards,

    Aishwarya