Part Number: TMS320F28386D
Tool/software:
Hello,
I have been working on the TMS320F28386D device and would like to get more information on the peripheral frames.
My main concerns are the following:
1) How are peripheral frames connected to the mains busses (Sys, DMA, CLA)?
2) Are the peripheral frames capable of servicing multiple transactions at the same time?
3) If 2) answer is no, what arbitration mechanism is in place to arbitrate between the different bus?
4) To which bus(es) is connected each peripheral frame? The Data sheet provides a diagram with connections but I would like to have more textual information about this.
5) Can two different bus (say CLA1 bus and CPU1 bus) access two different peripherals on two different peripheral frames at the same time?
More globally, is there a more detailed reference guide for peripheral frames for the TMS320F2838x family devices?
The Chapter 8.3 CLA, DMA, and CPU Arbitration or the TRM is not completely clear about those points.
Best regards,
Alexy Torres