This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28388D: Two Different Compilers in Project Files

Part Number: TMS320F28388D

Tool/software:

Greetings,

For our development, we are using CCS10.4 and Compiler v22.6.1.LTS.  We also do builds using automated tools running under a Command Prompt.  Those tools are taking the compiler identification from the codegenToolVersion value in the .ccsproject file.  In this project, that value is 20.2.5.LTS which is obviously different.  The v22.6.1.LTS version, which CCS is using, is from the .cproject file.  Are those two locations supposed to be different?  Should one change when the other changes?

Thank you,

Ed