Part Number: SM320F2808-EP
Other Parts Discussed in Thread: SPRC191, CONTROLSUITE, C2000WARE
Tool/software:
Hello,
We are looking to work on an older processor, the SM320F2808PZMEP. It is listed as supported by CCS from what we can tell, but there are no options to select the device in the latest CCS. As I understand the SM320 version of the part is functionally equivalent to the TMS320, and the part selection should be under the latter.
I've tried downloading an older version of CCS, version 10.2 which has the part selectable, however, when attempting to use any of the example code provided in SPRC191 I get a build error relating to not having XDAIS installed. When I look to install XDIAS, I only can find the linux tar.gz.
We do have the TMDSCNCD2808 development board, so what would be the easiest way to get going and compile a simple example project such as the GPIO setup? I.e. what CCS version and what dependencies do we need?
Thanks,
Steve