Other Parts Discussed in Thread: TMS320F28335
On TMS320F28335 processor, for those unused GPIO pins, shall they be connected to GND directly or through a resistor? Is a 2K ohm resistor ok to pull down?
If the unused GPIO is connected to GND directly, there is a concern that if the software accidently configures the pin to an output at development stage, then it might cause a damage to the pin or DSP. Maybe it's safer to use a pull-down resistor to connect the unused GPIO to GND. (I prefer pull-down than pull-up) The question is: what's the best value for the pull-down resistor? Any suggestions?
Thank you.