Part Number: TMS320F28035
Tool/software:
I have attached the code I am using to use SPI communication protocol to read the position data of the BLDC motor using EVAL - AD2S1210SDZ. The SPI communication is working fine, however no data is getting collected(posData).
#include "DSP28x_Project.h"
#include "DSP2803x_Device.h" // DSP2803x Header file Include File
#include "DSP2803x_Examples.h" // DSP2803x Examples Include File
#include "DSP2803x_CpuTimers.h" // CPU Timer header
#include "resolver.h"
typedef unsigned int bool;
#define true 1
#define false 0
volatile Uint16 transmittedData = 0x00;
volatile Uint16 receivedData;
volatile Uint16 posData; // Declare posData
volatile Uint16 velData; // Declare velData
volatile bool dataReceived = false;
void SPI_Write(Uint16 address, Uint16 data); // Function prototype
Uint16 SPI_Read(Uint16 address, Uint8 mode);
void SetMode(Uint16 mode);
void AD2S1210_Config(void);
void InitGpio(void);
void InitTimer(void);
void InitSPI(void);
void InitSpiGpio(void);
__interrupt void cpu_timer0_isr(void);
__interrupt void SPI_RX_ISR(void);
__interrupt void SPI_TX_ISR(void);
void main(void)
{
InitSysCtrl(); // Initialize the system control
InitSpiaGpio();
DINT; // Disable CPU interrupts
InitPieCtrl(); // Initialize the PIE control registers
IER = 0x0000; // Disable CPU interrupts
IFR = 0x0000; // Clear all CPU interrupt flags
InitPieVectTable(); // Initialize the PIE vector table
EALLOW;
PieVectTable.TINT0 = &cpu_timer0_isr; // Map ISR function
PieVectTable.SPIRXINTA = &SPI_RX_ISR;
PieVectTable.SPITXINTA = &SPI_TX_ISR;
EDIS;
InitGpio(); // Initialize GPIO
InitTimer(); // Initialize the timer
InitSPI(); // Initialize SPI
IER |= M_INT1; // Enable CPU INT1
PieCtrlRegs.PIEIER1.bit.INTx7 = 1; // Enable PIE Group 1 INT7
EINT; // Enable Global interrupt INTM
ERTM; // Enable Global real time interrupt DBGM
AD2S1210_Config(); // Configure AD2S1210
while(1)
{
// Main Loop
}
}
void InitGpio(void)
{
EALLOW;
GpioCtrlRegs.GPAMUX1.bit.GPIO0 = 0; // GPIO functionality
GpioCtrlRegs.GPADIR.bit.GPIO0 = 1; // GPIO0 as output
GpioCtrlRegs.GPAPUD.bit.GPIO1 = 0; // Enable pull-up on GPIO1
GpioDataRegs.GPASET.bit.GPIO1 = 1; // Load output latch
GpioCtrlRegs.GPAMUX1.bit.GPIO1 = 0; // GPIO1 = GPIO1
GpioCtrlRegs.GPADIR.bit.GPIO1 = 1; // GPIO1 as output
GpioCtrlRegs.GPAPUD.bit.GPIO3 = 0; // Enable pullup on GPIO3
GpioDataRegs.GPASET.bit.GPIO3 = 1; // Load output latch
GpioCtrlRegs.GPAMUX1.bit.GPIO3 = 0; // GPIO3 = GPIO3
GpioCtrlRegs.GPADIR.bit.GPIO3 = 1; // GPIO3 as output
/*GpioCtrlRegs.GPAPUD.bit.GPIO20 = 0; // Enable pull-up on GPIO20 (WR/FSYNC)
GpioDataRegs.GPASET.bit.GPIO20 = 1; // Load output latch
GpioCtrlRegs.GPAMUX2.bit.GPIO20 = 0;
GpioCtrlRegs.GPADIR.bit.GPIO20 = 1; // GPIO20 as output*/
GpioCtrlRegs.GPAPUD.bit.GPIO23 = 0; // Enable pull-up on GPIO23 (SAMPLE)
GpioDataRegs.GPASET.bit.GPIO23 = 1; // Load output latch
GpioCtrlRegs.GPAMUX2.bit.GPIO23 = 0; // GPIO3 = GPIO3
GpioCtrlRegs.GPADIR.bit.GPIO23 = 1; // GPIO23 as output
EDIS;
}
void InitTimer(void)
{
EALLOW;
CpuTimer0Regs.PRD.all = 600000; // Set timer period (3 ms)
CpuTimer0Regs.TCR.bit.TSS = 1; // Stop timer
CpuTimer0Regs.TCR.bit.TRB = 1; // Reload timer
CpuTimer0Regs.TCR.bit.TIE = 1; // Enable timer interrupt
CpuTimer0Regs.TCR.bit.TSS = 0; // Start timer
EDIS;
}
__interrupt void cpu_timer0_isr(void)
{
CpuTimer0.InterruptCount++;
// Toggle GPIO0
GpioDataRegs.GPATOGGLE.bit.GPIO0 = 1;
GpioDataRegs.GPATOGGLE.bit.GPIO23 = 1; //Sample pin toggling
// Enter Normal mode—position output
posData = SPI_Read(POS_LOW_ADDRESS, 0);
// Acknowledge this interrupt to receive more interrupts from group 1
PieCtrlRegs.PIEACK.all = PIEACK_GROUP1;
}
__interrupt void SPI_RX_ISR(void)
{
receivedData = SpiaRegs.SPIRXBUF; // Read received data
dataReceived = true; // Set flag indicating data received
PieCtrlRegs.PIEACK.all = PIEACK_GROUP6; // Acknowledge interrupt
}
__interrupt void SPI_TX_ISR(void)
{
SpiaRegs.SPITXBUF = transmittedData; // Transmit data
PieCtrlRegs.PIEACK.all = PIEACK_GROUP6; // Acknowledge interrupt
}
// file end
void InitSPI(void)
{
EALLOW;
// Reset SPI
SpiaRegs.SPICCR.bit.SPISWRESET = 0;
// Initialize SPI-A
SpiaRegs.SPICCR.all = 0x000F; // Reset on, rising edge, 16-bit char bits
SpiaRegs.SPICTL.all = 0x0006; // Enable master mode, normal phase, enable talk
SpiaRegs.SPIBRR = 0x0005; // Baud rate for SPI clock
SpiaRegs.SPICCR.all = 0x008F; // Relinquish SPI from reset
SpiaRegs.SPIPRI.bit.FREE = 1; // Set so breakpoints don't disturb xmission
// Enable SPI
SpiaRegs.SPICCR.bit.SPISWRESET = 1;
// Enable SPI interrupts
SpiaRegs.SPICTL.bit.SPIINTENA = 1; // Enable SPI interrupt
//PieCtrlRegs.PIEIER6.bit.INTx1 = 1; // Enable PIE Group 6, INT1 (SPIA RX)
//PieCtrlRegs.PIEIER6.bit.INTx2 = 1; // Enable PIE Group 6, INT2 (SPIA TX)
IER |= M_INT6; // Enable CPU INT6 (for SPI)
EDIS;
}
//---------------------------------------------------------------------------
// Example: InitSpiGpio:
//---------------------------------------------------------------------------
// This function initializes GPIO pins to function as SPI pins
//
void InitSpiGpio()
{
InitSpiaGpio();
}
void InitSpiaGpio()
{
EALLOW;
// Enable internal pull-up for the selected pins
GpioCtrlRegs.GPAPUD.bit.GPIO16 = 0; // Enable pull-up on GPIO16 (SPISIMOA)
GpioCtrlRegs.GPAPUD.bit.GPIO17 = 0; // Enable pull-up on GPIO17 (SPISOMIA)
GpioCtrlRegs.GPAPUD.bit.GPIO18 = 0; // Enable pull-up on GPIO18 (SPICLKA)
GpioCtrlRegs.GPAPUD.bit.GPIO19 = 0; // Enable pull-up on GPIO19 (SPISTEA)
// Set qualification for selected pins to asynch only
GpioCtrlRegs.GPAQSEL2.bit.GPIO16 = 3; // Asynch input GPIO16 (SPISIMOA)
GpioCtrlRegs.GPAQSEL2.bit.GPIO17 = 3; // Asynch input GPIO17 (SPISOMIA)
GpioCtrlRegs.GPAQSEL2.bit.GPIO18 = 3; // Asynch input GPIO18 (SPICLKA)
GpioCtrlRegs.GPAQSEL2.bit.GPIO19 = 3; // Asynch input GPIO19 (SPISTEA)
// Configure SPI-A pins using GPIO regs
GpioCtrlRegs.GPAMUX2.bit.GPIO16 = 1; // Configure GPIO16 as SPISIMOA
GpioCtrlRegs.GPAMUX2.bit.GPIO17 = 1; // Configure GPIO17 as SPISOMIA
GpioCtrlRegs.GPAMUX2.bit.GPIO18 = 1; // Configure GPIO18 as SPICLKA
GpioCtrlRegs.GPAMUX2.bit.GPIO19 = 1; // Configure GPIO19 as SPISTEA
GpioDataRegs.GPACLEAR.bit.GPIO19 = 1;
EDIS;
}
//===========================================================================
// End of file.
//===========================================================================
// resolver.c
#include "DSP28x_Project.h"
#include "DSP2803x_Spi.h"
#include "resolver.h"
void SPI_Write(Uint16 address, Uint16 data) {
SetMode(3);
DELAY_US(20);
while (SpiaRegs.SPISTS.bit.BUFFULL_FLAG); // Wait if buffer is full
SpiaRegs.SPITXBUF = address; // Transmit data
while(SpiaRegs.SPISTS.bit.INT_FLAG != 1)
{
/* wait till SPI has completed sending or receiving */
}
while (SpiaRegs.SPISTS.bit.BUFFULL_FLAG); // Wait if buffer is full
SpiaRegs.SPITXBUF = data; // Transmit data
SetMode(0);
}
Uint16 SPI_Read(Uint16 address, Uint8 mode) {
SetMode(3);
DELAY_US(20);
while (SpiaRegs.SPISTS.bit.BUFFULL_FLAG); // Wait if buffer is full
SpiaRegs.SPITXBUF = address; // Transmit address
SetMode(mode);
while (!SpiaRegs.SPISTS.bit.INT_FLAG); // Wait for data to be received
receivedData = SpiaRegs.SPIRXBUF; // Read received data
return receivedData;
}
void SetMode(Uint16 mode) {
switch (mode) {
case 0: // Normal mode—position output
GpioDataRegs.GPACLEAR.bit.GPIO1 = 1; // Set A0 low
GpioDataRegs.GPACLEAR.bit.GPIO3 = 1; // Set A1 low
break;
case 1: // Normal mode—velocity output
GpioDataRegs.GPACLEAR.bit.GPIO1 = 1; // Set A0 low
GpioDataRegs.GPASET.bit.GPIO3 = 1; // Set A1 high
break;
case 2: // Reserved
GpioDataRegs.GPASET.bit.GPIO1 = 1; // Set A0 high
GpioDataRegs.GPACLEAR.bit.GPIO3 = 1; // Set A1 low
break;
case 3: // Configuration mode
GpioDataRegs.GPASET.bit.GPIO1 = 1; // Set A0 high
GpioDataRegs.GPASET.bit.GPIO3 = 1; // Set A1 high
break;
default:
// Handle invalid mode
break;
}
}
void AD2S1210_Config(void) {
SPI_Write(AD2S1210_EXCIT_FREQ, 5); // frequency control word for 10 kHz
}
//resolver.c ends here
// resolver.h #ifndef RESOLVER_H #define RESOLVER_H #define POS_HIGH_ADDRESS 0x80 // D15 to D8 (Read only) #define POS_LOW_ADDRESS 0x81 // D7 to D0 (Read only) //#define VEL_HIGH_ADDRESS 0x82 // D15 to D8 (Read only) #define VEL_LOW_ADDRESS 0x83 // D7 to D0 (Read only) #define AD2S1210_LOS_THRD 0x88 #define AD2S1210_DOS_OVR_THRD 0x89 #define AD2S1210_DOS_MIS_THRD 0x8A #define AD2S1210_DOS_RST_MAX_THRD 0x8B #define AD2S1210_DOS_RST_MIN_THRD 0x8C #define AD2S1210_LOT_HIGH_THRD 0x8D #define AD2S1210_LOT_LOW_THRD 0x8E #define AD2S1210_EXCIT_FREQ 0x91 #define AD2S1210_CONTROL 0x92 #define AD2S1210_SOFT_RESET 0xF0 #define AD2S1210_FAULT 0xFF extern volatile Uint16 receivedData; // Declare receivedData as extern void SPI_Write(Uint16 address, Uint16 data); Uint16 SPI_Read(Uint16 address, Uint8 mode); void SetMode(Uint16 mode); void AD2S1210_Config(void); #endif // RESOLVER_H