Part Number: TMS320F280041C
Other Parts Discussed in Thread: MOTORWARE,
Tool/software:
Greetings! I have a working PCB using your TMS320F280041C. It is a frequency inverter. So I made a second pcb absolutely the same as the first one(they came together 5 pcs). But this time only one of the selected ADC channels is responding. I am using A2(pin 2), A6(pin 6), A8(pin 37), A10(pin 40), B2(pin 7), B4(pin 39), C1(pin 29). I haven`t made any changes in the hal.c of the motorware library form the working vertion. The PGA init is total empty.
But only 1 or 2 pins seems to respond and actually calculate the voltage value. Any suggestions what can cause this?
I changed the uC with brand new(all the same it wasn`t demaged)...