Other Parts Discussed in Thread: C2000WARE
Tool/software:
hi, am working on TMS320F28377D microcontroller, i got to one requirement regarding bit flip(multiple bit upset) in internal flash so i we were planning to copy paste the program in multiple location in internal
so, please give me example code or mechanism to copy and paste in multiple location in microcontroller
please find the memory partitioning of our software
|
Region |
Address |
Length (Bytes) in Decimal |
DMM Microcontroller used |
Purpose |
|
BEGIN |
0x080000 |
2 Bytes |
2 Bytes(100%) |
Bootloader entry point for "Boot to Flash". |
|
RAMM1 |
0x000400 |
1016 Bytes |
256 Bytes(25%) |
runtime data for initialization and stack. |
|
RAMLS0 |
0x008000 |
2048 Bytes |
350 Bytes(17%) |
Run program CPU1 tasks. |
|
RAMLS5 |
0x00A800 |
2048 Bytes |
427 Bytes (20%) |
Shared tasks or configuration. |
|
Region |
Address |
Length (Bytes) |
DMM Microcontroller used |
Purpose |
|
Flash Section B |
0x082000 |
8192 Bytes |
5753 Bytes(70%) |
Application program (CPU1) |
|
Flash Section D |
0x086000 |
8192 Bytes |
350 Bytes(4%) |
Redundant data or fail-safe. |
|
Flash Section E |
0x088000 |
32768 Bytes |
36 Bytes(0.11%) |
Calibration and configuration data. |
|
Flash Section F |
0x090000 |
32768 Bytes |
170 Bytes(0.52%) |
Logging and analytics. |
regards
J.Muniniteesh