This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28027F: TMS320F28027with DRV8301 to run bldc motor

Part Number: TMS320F28027F
Other Parts Discussed in Thread: MOTORWARE

Tool/software:

Hi 

I installed Motor Ware and imported Project Lab 2C into CCS. I modified the motor [A2212/13T] parameters in the user.h file, but after flashing the code to the board, the motor isn't running. I'm not using InstaSPIN GUI process. Could anyone guide me?

#define USER_MOTOR_RES_EST_CURRENT (3.0) // A - 10-30% of
#define USER_MOTOR_IND_EST_CURRENT (-3.0) // A - 10-30% of
#define USER_MOTOR_MAX_CURRENT (20.0) // A - 30~150% of
#define USER_MOTOR_FLUX_EST_FREQ_Hz (20.0) // Hz - 10~30% rated

  • Please take a look at the lab user's guide, and follow the instruction to run or identify the motor.

    The lab user's guide  (instaspin_labs.pdf) is at the folder below. to run the related lab projects.

    \ti\motorware\motorware_1_01_00_18\docs\labs