This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28P650DK: Problems connecting to device after programming

Part Number: TMS320F28P650DK

Tool/software:

Dear Forum,

I have developed some custom digital control boards based around the TMS320F28P650DK9ZEJ part. The prototype board I have been using for a few months has been working well but I'm not able to connect to it via the XDS200 now. I receive an -2131 error as shown below:-

I can't even connect to the board using the 'test connection' tool under the new configuration tool. The C2000 part is hosted on a small daughter board so I built another one and powered it up separately from the main system. I was able to connect to the device straightaway and upload my test code. However, on that new board now I can no longer connect to the C2000 part.

Any idea on why this might happen? I do have another spare controller board but am reluctant to program until I know what is happening here. Just a reminder, the first board was working without issue for months just prior to this issue.

Thanks,

Iain