Part Number: TMS320F2812
Other Parts Discussed in Thread: C2000WARE
Tool/software:
Hi
I need Code Composer Studio with bios_setupwin32_5_33_06, since in the below mentioned download link CCS is coming with bios_setupwin32_5_33_05. My Older projects have used 32_5_33_06 i need that. I have tried updating the bios version in component manager after installing bios_setupwin32_5_33_06.exe manually. It's not at all reflecting in my windows 11. if I enable bios_setupwin32_5_33_06 in component manager, both version are not able to select and i am unable to compile after that. I need help in this and kindly provide your suggestion and download link.
For alternate option for Code Composer Studio 3.3, which version i can use without modifying my current project files that i am using.