This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F280039: C2000 C/C++ Compiler user statistics: where to find them?

Part Number: TMS320F280039


Tool/software:

I'm compiling the SAFETI_CQKIT qualification documents, which require the software download statistics to be updated with the latest from TI, specifically for the C2000 C/C++ Compiler.

The above is an example extracted from the Tool Qualification Plan supplied in the SAFETY_CQKIT (sic est), where it has to be filled with real/specific data.

Where do I find the above data for the C2000 C/C++ Compiler version 22.6.2.LTS?

  • Luca,

    The C2000 22.6.2 compiler is very new.  I see 262 downloads.  Note that it will also be bundled in the upcoming Code Composer Studio v20.2.0 releasee which will have tens of thousands of downloads.

    Regards,

    John

  • John, I understand that's a new release, although I can't find the download statistics.

    Focusing on the older 20.2.7.LTS (August 2022) still I can't find the download statistics either: maybe I'm looking in the wrong place?

    [EDIT]

    Note: for the needs of the Tool Qualification Plan in the SAFETI_CQKIT I have to mention download numbers starting from the initial version. In the first case, this accounts for 22.6.0.LTS onward, then the numbers could be significant also for the 22.6.x series.
    I just can't find on the site where (and how) I can retrieve a table like the one pictured - the total of downloads by file and by period.

  • maybe I'm looking in the wrong place?

    This information is not posted publicly.

    Focusing on the older 20.2.7.LTS

    273 downloads since January 2024.  The data I can access doesn't go back farther than that.  Is this good enough for your purposes?

    Thanks and regards,

    -George

  • Is this good enough for your purposes?

    Hi George,
    maybe not, given the example of tabular data in the TI documentation. Anyway, knowing now that's not publicly available data, I submitted a support ticket, just to know better about it.

    I started from the forum, thinking it was just a public site page that I was unable to find.

    Thanks

  • Since I've been told by TI Customer Support that this forum is the most suitable place for this issue, I will go a bit further.

    Planning to use version 20.2.7.LTS, I would then need the download data for versions from 20.2.0.LTS through 20.2.7.LTS. From the TI documentation in my original posting, it looks to be available (somewhat) in a table form, that I can embed in my edited document. How can I get it?

  • Hello,

    Please note that due to some vacations/holidays, it may be a few days to get a response.

    Thank you

    ki

  • Luca,

    The screenshot of the table is from one or our internal stats tools.  For C2000 20.2.x this is the data for 2024 and 2025

    Regards,

    John

  • John,

    thank you for the screenshot, that's exactly what is needed by the documentation.

    Luca