Part Number: TMS320F28377D
Tool/software:
Hi Expert
Customer reports the issue with CCS6.2 and v15.12.3.LTS compiler. once the --opt_level set to 0/1/2 the issue can be reproduced, set to off the issue cannot be reproduced
below are the actions customer take to reproduce the issue:
1. claim a structure like this:
{
Var1
Var2
....
} Structure 1
2. claim a structure nest Structure1 like this:
{
Var1
Var2
....
Structure 1 instance
& function handler
&Structure 2 address
} Structure_2
3. Claim the array Structure_2[N], and write a for loop to select the largest Var1 in Structure_2[N], for example:
Temp = 0
for (i = 0; i<N; i++)
{
if Temp < Structure_2[N].Var1 {
Temp = Structure_2[N].Var1
}
}
4. set --opt_level to any 0/1/2 level, build and run the project, the variables value in Structure_2 will be changed randomly.
5. if set --opt_level to off, or block the for loop or write the compare statement N times instead of for loop, the issue won't happen.
Could you please share some advices to debug this issue?
Thanks
Joe