Part Number: TMS320F28P659DH-Q1
Tool/software:
Hi experts,
Good day! I am asking for customer.
1. My customer would like to confirm that when the CLA is writing 32-bit data to share RAM, only the first 16-bit write was completed and then 16 bits were not written. At this point CPU1 is going to read the CLA data, will it read only the updated first 16-bit data? Or wait for the CLA to completely update this 32-bit data before CPU1 reads?
2. In TRM it's showed that CLA bus can perform 16 or 32-bit read/write. 16 or 32-bit read/write means that if access 16bit data, then will use 16bit data bus. If access 32bit data, then will use 32bit data bus. Does it has2 buses or 1 bus which is compatible A and B?
Could you help to check this? Thanks!
Best Regards
Kita