Part Number: TMS320F28P650DK
Other Parts Discussed in Thread: UNIFLASH
Tool/software:
Hi Expert
Customer report that CCS will report the below issue during F28P65 program download:

The CCS version is 12.8.1, emulator version is xds100v2, cmd file is attached:
MEMORY
{
BEGIN : origin = 0x080000, length = 0x000008 // Update the codestart location as needed
BOOT_RSVD : origin = 0x000002, length = 0x0001AF /* Part of M0, BOOT rom will use this for stack */
//RAMM0 : origin = 0x0001B1, length = 0x00024F
//RAMM1 : origin = 0x000400, length = 0x000400
RAMM1 : origin = 0x0001B1, length = 0x00064F
RAMD_DATA1 : origin = 0x00C000, length = 0x004000
RAMD_DATA2 : origin = 0x01A000, length = 0x008000
RAMLS_Prog : origin = 0x008000, length = 0x003000
RAMLS6 : origin = 0x00B000, length = 0x000800
RAMLS7 : origin = 0x00B800, length = 0x000800
RAMLS8 : origin = 0x022000, length = 0x002000 // When configured as CLA program use the address 0x4000
RAMLS9 : origin = 0x024000, length = 0x002000 // When configured as CLA program use the address 0x6000
RAMGS_Prog : origin = 0x010000, length = 0x006000
RAMGS3 : origin = 0x016000, length = 0x002000
RAM_data : origin = 0x018000, length = 0x001C00
RAM_DMA1 : origin = 0x019C00, length = 0x000100
RAM_DMA2 : origin = 0x019D00, length = 0x000100
RAM_DMA3 : origin = 0x019E00, length = 0x000100
RAM_DMA4 : origin = 0x019F00, length = 0x000100
/* Flash Banks (128 sectors each) */
FLASH_IAP_CODE : origin = 0x080008, length = 0x0FFF8
FLASH_IAP_DATA : origin = 0x090000, length = 0x10000
APP_HEAD_KEY : origin = 0x0A0000, length = 0x00008
FLASH_APP_ENTRY : origin = 0x0A0008, length = 0x00008
FLASH_APP_CODE : origin = 0x0A0010, length = 0x3FBE8
APP_END_KEY : origin = 0x0DFBF8, length = 0x00008
APP_STORE_ID : origin = 0x0DFC00, length = 0x00400
CPU1TOCPU2RAM : origin = 0x03A000, length = 0x000400
CPU2TOCPU1RAM : origin = 0x03B000, length = 0x000400
CLATOCPURAM : origin = 0x001480, length = 0x000080
CPUTOCLARAM : origin = 0x001500, length = 0x000080
CLATODMARAM : origin = 0x001680, length = 0x000080
DMATOCLARAM : origin = 0x001700, length = 0x000080
CANA_MSG_RAM : origin = 0x049000, length = 0x000800
CANB_MSG_RAM : origin = 0x04B000, length = 0x000800
RESET : origin = 0x3FFFC0, length = 0x000002
}
SECTIONS
{
.text : > FLASH_APP_CODE, ALIGN(8)
.cinit : > FLASH_APP_CODE, ALIGN(8)
.switch : > FLASH_APP_CODE, ALIGN(8)
.reset : > RESET, TYPE = DSECT /* not used, */
bootstart : > BEGIN
codestart : > FLASH_APP_ENTRY
APP_HEAD : > APP_HEAD_KEY
APP_END : > APP_END_KEY
IAP_DATA : > FLASH_IAP_DATA
IAP_CODE : > FLASH_IAP_CODE
.stack : > RAMM1
#if defined(TI_EABI)
.bss : > RAMD_DATA2
.bss:output : > RAMD_DATA1
.data : > RAMGS3
.sysmem : > RAMD_DATA1
.init_array : > FLASH_APP_CODE, ALIGN(8)
.const : > FLASH_APP_CODE, ALIGN(8)
#else
.pinit : > FLASH_APP_CODE, ALIGN(8)
.econst : > FLASH_APP_CODE, ALIGN(8)
.ebss : > RAMD_DATA2
.esysmem : > RAMD_DATA1
#endif
RamDataD : > RAM_data, type=NOINIT
ADCAData : > RAM_DMA1, type=NOINIT
ADCBData : > RAM_DMA2, type=NOINIT
ADCCData : > RAM_DMA3, type=NOINIT
ADCDData : > RAM_DMA4, type=NOINIT
MSGRAM_CPU1_TO_CPU2 > CPU1TOCPU2RAM, type=NOINIT
MSGRAM_CPU2_TO_CPU1 > CPU2TOCPU1RAM, type=NOINIT
#if defined(TI_EABI)
.TI.ramfunc : {} LOAD = FLASH_APP_CODE,
RUN = RAMGS_Prog,
LOAD_START(RamfuncsLoadStart),
LOAD_SIZE(RamfuncsLoadSize),
LOAD_END(RamfuncsLoadEnd),
RUN_START(RamfuncsRunStart),
RUN_SIZE(RamfuncsRunSize),
RUN_END(RamfuncsRunEnd),
ALIGN(8)
#else
.TI.ramfunc : {} LOAD = FLASH_APP_CODE,
RUN = RAMGS_Prog,
LOAD_START(_RamfuncsLoadStart),
LOAD_SIZE(_RamfuncsLoadSize),
LOAD_END(_RamfuncsLoadEnd),
RUN_START(_RamfuncsRunStart),
RUN_SIZE(_RamfuncsRunSize),
RUN_END(_RamfuncsRunEnd),
ALIGN(8)
#endif
/* CLA specific sections */
#if defined(TI_EABI)
/* CLA specific sections /
Cla1Prog : LOAD = FLASH_APP_CODE,
RUN = RAMLS_Prog,
LOAD_START(Cla1ProgLoadStart),
RUN_START(Cla1ProgRunStart),
LOAD_SIZE(Cla1ProgLoadSize),
ALIGN(4)
#else
/ CLA specific sections */
Cla1Prog : LOAD = FLASH_APP_CODE,
RUN = RAMLS_Prog,
LOAD_START(_Cla1ProgLoadStart),
RUN_START(_Cla1ProgRunStart),
LOAD_SIZE(_Cla1ProgLoadSize),
ALIGN(4)
#endif
Cla1ToCpuMsgRAM : > CLATOCPURAM
CpuToCla1MsgRAM : > CPUTOCLARAM
#ifdef CLA_C
// CLA C compiler sections
// Must be allocated to memory the CLA has write access to
.scratchpad : > RAMLS6
.bss_cla : > RAMLS6
cla_shared : > RAMLS6
#endif
#if defined(TI_EABI)
.const_cla : LOAD = FLASH_APP_CODE,
RUN = RAMLS6,//RAMLS1,
RUN_START(Cla1ConstRunStart),
LOAD_START(Cla1ConstLoadStart),
LOAD_SIZE(Cla1ConstLoadSize),
ALIGN(4)
#else
.const_cla : LOAD = FLASH_APP_CODE,
RUN = RAMLS6,//RAMLS1,
RUN_START(_Cla1ConstRunStart),
LOAD_START(_Cla1ConstLoadStart),
LOAD_SIZE(_Cla1ConstLoadSize),
ALIGN(4)
#endif
CLA1mathTables : > RAMLS7
//Load tables to Flash and copy over to RAM
#if defined(TI_EABI)
CLA1mathTables : LOAD = FLASH_APP_CODE,
RUN = RAMLS7,
RUN_START(CLA1mathTablesRunStart),
LOAD_START(CLA1mathTablesLoadStart),
LOAD_SIZE(CLA1mathTablesLoadSize)
#else
CLA1mathTables : LOAD = FLASH_APP_CODE,
RUN = RAMLS7,
RUN_START(_CLA1mathTablesRunStart),
LOAD_START(_CLA1mathTablesLoadStart),
LOAD_SIZE(_CLA1mathTablesLoadSize)
#endif
}
the same output file can be downloaded with xds110 USB + CCS properly, and with xds100v2+UNIFLASH8.5.0 properly.
before dowload, if verify the device with UNIFLASH, the UNIFLASH+XDS100V2 will report error:
![]()
but the program can be downloaded successfully:

I think it may be the compatible issue between xds100v2 and F28P65, Could you please help to recommend the emulator and standard program process for F28P65?
Thanks
Joe