Part Number: TMS320F28069M
Other Parts Discussed in Thread: MOTORWARE
Tool/software:
I have setup the Lab 3a of Launchpadxl-TMS320F28069M along with Boosterxl-DRV8301 with and BLDC motor , Everything seems fine with default settings that Motorware provides, But when i try to change the default parameters in the
user_j1.h
#elif (USER_MOTOR == Anaheim_BLY172S)
#define USER_MOTOR_TYPE MOTOR_Type_Pm
#define USER_MOTOR_NUM_POLE_PAIRS (5) <-------my motor values
#define USER_MOTOR_Rr (NULL)
#define USER_MOTOR_Rs (3.3) <-----------New Value (no problem)
#define USER_MOTOR_Ls_d (0.05) <------------Error in GUI (Unable to enable the system tick make)
#define USER_MOTOR_Ls_q (0.05) <------------Error in GUI (Unable to enable the system tick make)
#define USER_MOTOR_RATED_FLUX (0.03279636)
User Motor Values
0.362524v/Hz
L-L Resistance -6.6 Ohm
L-L Inductance 20.56mH
Voltage Constant 37V/Krpm