This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28377D: UniFlash, Blank Check with dslite (command line, batch)

Part Number: TMS320F28377D
Other Parts Discussed in Thread: UNIFLASH,

Tool/software:

Hi,

With the UniFlash it is possible to do a "Blank Check".
Is it also possible with a batch file? If so, how?

Thanks and best regards,

Patrick

  • Hi Patrick,

    Yes, it is possible to do a "Blank Check" using dslite. In the generated package of Uniflash, it will create the dslite-C28xx_CPU1.bat file. The set GENERATED_COMMAND parameter can be modified by adding -b BlankCheck as an argument to perform the Blank Check before operations begin. 

    Uniflash Flash Mode Options for reference on list of arguments. 

    Thanks and regards,

    Charles

  • Hi Charles,

    Thanks. It works.
    For others who have to do the same:
    The GENERATED_COMMAND needs to be modified as follows:

    set GENERATED_COMMAND=-c user_files/configs/tms320f28377d.ccxml -l user_files/settings/generated.ufsettings -s VerifyAfterProgramLoad="No verification" -b BlankCheck

    Regards,
    Patrick