Other Parts Discussed in Thread: SYSCONFIG, C2000WARE
Tool/software:
Hello,
I am trying to use TMS320F28379D as an inverter, but I keep getting error messages when I try to use the EPWM example. Here are the error messages I get:
[36]>> Compilation failure
[37]subdir_rules.mk:38: recipe for target 'lab_main.obj' failed
[38]"../lab_main.c", line 71: error #20: identifier "INT_myADC0_1_INTERRUPT_ACK_GROUP" is undefined
[39]"../lab_main.c", line 72: error #20: identifier "myADC0_BASE" is undefined
[40]"../lab_main.c", line 74: error #20: identifier "myADC0_RESULT_BASE" is undefined
[41]"../lab_main.c", line 74: error #20: identifier "myADC0_SOC0" is undefined
[42]"../lab_main.c", line 84: error #20: identifier "myBoardLED0_GPIO" is undefined
[43]"../lab_main.c", line 113: error #20: identifier "myEPWM0_BASE" is undefined
[44]"../lab_main.c", line 117: error #66: expected a ";"
[45]At end of source: warning #12-D: parsing restarts here after previous syntax error
[46]At end of source: error #68: expected a "}"
[47]8 errors detected in the compilation of "../lab_main.c".
[48]gmake: *** [lab_main.obj] Error 1
[49]Building file: "../device/F2837xD_CodeStartBranch.asm"
[50]Invoking: C2000 Comp
I think I am missing a library for this example but I do not know where I can download this library. Can I have some help with this?