Part Number: TMS320F28P650DK
Other Parts Discussed in Thread: SYSCONFIG, C2000WARE
Tool/software:
Hi everyone,
I'm using SysConfig to generate the CMD (linker command) file for my project. While it works overall, I'm running into a few issues and warnings that I'd like help resolving.
1. Flash Assignment Warnings
I've defined a custom memory region that currently maps only to FLASH BANK 1, and I plan to extend it later to include BANK 2 as well. I'm assigning this region to standard sections like .text, .binit, .ovly, .cinit, .init_array, .const, switch, and some user-defined sections.
However, SysConfig generates multiple warnings like:
"The memcfg module is needed on CPU1 to assign FLASH."
This is confusing because I have already configured the memcfg module:
-
FLASH BANKS 0, 1, and 2 are assigned to CPU1
-
FLASH BANKS 3 and 4 are assigned to CPU2
Strangely, when I use predefined flash regions (like the default ones SysConfig provides), these warnings disappear. Is this a known issue with custom memory regions? Or is there something I’m missing in the configuration?


2. CPU-to-CLA Message RAM Warning
I'm also seeing a warning related to CPU to CLA message RAM configuration, but the setup seems correct from my end.
Memcfg module must be enabled for complete error checking.

3. Assigning a Symbol to a Fixed Memory Address
Unrelated to the above, but I’m also trying to replicate this kind of memory definition in my linker script:
MAIN_FIRMWARE_VERSION : origin = 0x0FFFD0, length = 0x000010
Is there a clean way to declare this using SysConfig, or is it better to define such regions manually in a separate CMD file?
Thanks in advance for your help! Let me know if more details are needed.