Part Number: TMS320F280049C
Other Parts Discussed in Thread: SYSCONFIG, C2000WARE
Tool/software:
Hi,
I am using 56RSH package, with the below code, as suggested I am not using sysconfig
#include "driverlib.h"
#include "device.h"
#include "board.h"
// PGA instance for ADCIN2
#define PGA_NUMBER_3 3U
void initADC(void);
void initPGA(void);
void initSOC(void);
void main(void)
{
uint16_t adcResult;
float voltage;
// Initialize device clock and peripherals
Device_init();
// GPIO setup (not needed for C2 since it's analog-only, but kept for consistency)
Device_initGPIO();
// Optional: Board init (can be removed if not using Board.c/.h)
Board_init();
// Enable ADCC
SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_ADCC);
// Initialize ADC, PGA, and SOC
initADC();
initPGA();
initSOC();
while (1)
{
// Trigger ADC conversion on SOC2
ADC_forceSOC(ADCC_BASE, ADC_SOC_NUMBER2);
// Wait for conversion to complete
while (!ADC_getInterruptStatus(ADCC_BASE, ADC_INT_NUMBER1)) {}
// Clear the interrupt flag
ADC_clearInterruptStatus(ADCC_BASE, ADC_INT_NUMBER1);
// Read ADC result
adcResult = ADC_readResult(ADCCRESULT_BASE, ADC_SOC_NUMBER2);
// Convert ADC value to voltage (assuming 3.3V ref)
voltage = ((float)adcResult * 3.3f) / 4095.0f;
DEVICE_DELAY_US(100000); // Delay for observation (100ms)
}
}
void initADC(void)
{
// Set VREF to internal 3.3V
ADC_setVREF(ADCC_BASE, ADC_REFERENCE_INTERNAL, ADC_REFERENCE_3_3V);
// Set ADC clock divider
ADC_setPrescaler(ADCC_BASE, ADC_CLK_DIV_4_0);
// Set EOC to trigger interrupt at end of conversion
ADC_setInterruptPulseMode(ADCC_BASE, ADC_PULSE_END_OF_CONV);
// Enable ADC converter
ADC_enableConverter(ADCC_BASE);
DEVICE_DELAY_US(1000); // Delay for ADC stabilization
}
void initPGA(void)
{
// Enable PGA3 (attached to ADCIN2)
PGA_enable(PGA3_BASE );
// Set gain to 3x (choose PGA_GAIN_3, _6, or _12)
PGA_setGain(PGA3_BASE , PGA_GAIN_3);
}
void initSOC(void)
{
// Configure SOC2 on ADCC to sample from ADCIN2 (via PGA3)
ADC_setupSOC(ADCC_BASE, ADC_SOC_NUMBER2,
ADC_TRIGGER_SW_ONLY, ADC_CH_ADCIN2, 14);
// Link interrupt 1 to SOC2 EOC
ADC_setInterruptSource(ADCC_BASE, ADC_INT_NUMBER1, ADC_SOC_NUMBER2);
ADC_enableInterrupt(ADCC_BASE, ADC_INT_NUMBER1);
ADC_clearInterruptStatus(ADCC_BASE, ADC_INT_NUMBER1);
}
Now, the voltage is not coming as expected in custom board.